|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the width for a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. |
|
Units |
Position counts or microseconds depending on CMPx.WIDTHTYPE on pg. 1. If CMPx.WIDTHTYPE = 0 (position counts), then units depend on CMPx.SOURCE (see table below). |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 to 18,446,744,073,709,551,615 (position counts) |
|
Default Value |
0 |
|
Data Type |
Argument 1:Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Units
If CMPx.WIDTHTYPE = 0 (position counts),determine units with the following table.
| CMPx.SOURCE | Units |
|---|---|
| 0 (FB1) | Depends on FB1.PUNIT on pg. 1 or custom units. |
| 1 (FB2) | Depends on FB2.PUNIT on pg. 1 or custom units. |
| 2 (FB3) | Depends on FB2.PUNIT on pg. 1 or custom units. |
| 3 (PL.FB) | Depends on UNIT.PLINEAR
or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts Linear: counts, mm, µm, (custom units), 16-bit counts |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| PDMM | Revision DB or higher |
| AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material | Revision DA or higher |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34ABh/1 | CMP0.WIDTH 0 | M_01-13-00-000 | |
| 34AAh/2 | CMP0.WIDTH 1 | ||
| 34AAh/3 | CMP0.WIDTH 2 | ||
| 34AAh/4 | CMP0.WIDTH 3 | ||
| 34AAh/5 | CMP0.WIDTH 4 | ||
| 34AAh/6 | CMP0.WIDTH 5 | ||
| 34AAh/7 | CMP0.WIDTH 6 | ||
| 34AAh/8 | CMP0.WIDTH 7 | ||
|
34BBh/1 |
CMP1.WIDTH 0 | ||
|
34BAh/2 |
CMP1.WIDTH 1 | ||
|
34BAh/3 |
CMP1.WIDTH 2 | ||
|
34BAh/4 |
CMP1.WIDTH 3 | ||
|
34BAh/5 |
CMP1.WIDTH 4 | ||
|
34BAh/6 |
CMP1.WIDTH 5 | ||
|
34BAh/7 |
CMP1.WIDTH 6 | ||
|
34BAh/8 |
CMP1.WIDTH 7 | ||
Description
Use this keyword to set the width for a Compare setpoint. The width defines for how much time or for how many position counts a pulse will be generated once a setpoint is active.
If a pulse width's type is in microseconds, the resolution is as follows:
| Width | Resolution |
|---|---|
| 0 to 65,535 μs | μs |
| 65,536 μs to 65.535 s | ms |
CMPx.WIDTH must be set before CMPx.SETPOINT on pg. 1.
Example
The following example sets the width type of setpoint 7 to microseconds, and the width of setpoint 7 to 1000 microseconds.
-->CMP0.WIDTHTYPE 7 1
-->CMP0.WIDTH 7 1000
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|