This content is not applicable to KAS, using either a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
mA |
|
Range |
Argument 1: 0 to 8,191 Argument 2: 1.628 * DRV.IPEAK on pg. 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-14-06-001 |
Description
Reads or writes to the cogging compensation table.
Examples
Reads the full table:
COGCOMP.CORRECTIONTABLE
Reads the compensation value for index "x":
COGCOMP.CORRECTIONTABLE x
Writes the value "y" to the table at index "x":
COGCOMP.CORRECTIONTABLE x y
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|