You are here: Tools > AKD into KAS > Workbench Reference > CS.STATE

CS.STATE

General Information

Type

R/O Parameter

Description

Returns the internal status of the controlled stop process.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3441h on pg. 1/0

M_01-00-00-000

Description

CS.STATE returns the internal state machine value of the controlled stop.

0 = controlled stop is not occurring.

1 = controlled stop is occurring

Related Topics

Controlled Stop on pg. 1

Digital Inputs and Outputs on pg. 1

Fault and Warning Messages on pg. 1

CS.DEC on pg. 1, CS.VTHRESH on pg. 1, CS.TO on pg. 1DRV.DISMODE on pg. 1, DRV.DISSOURCES on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™