You are here: Tools > AKD into KAS > Workbench Reference > DRV.CLRFAULTS

DRV.CLRFAULTS

General Information

Type

Command

Description

Tries to clear all active faults in the drive.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Description

When DRV.CLRFAULTS is sent, the drive will try to clear all active faults. When a fault occurs, the fault is registered in the drive fault handler. DRV.CLRFAULTS clears the fault from the drive fault handler. However, if the fault still exists in the system, DRV.CLRFAULTS fails and the fault is re-registered in the fault handler.

If the DRV.CLRFAULTS succeeds, then the reply to DRV.FAULTS states that no faults exist. If the condition that triggered the fault is still present, the fault condition will remain.

See Fault and Warning Messages on pg. 1 for details regarding the behavior of individual faults.

Note that executing a drive disable (DRV.DIS on pg. 1) followed by a drive enable (DRV.EN on pg. 1) has the same effect as executing DRV.CLRFAULTS.

Related Topics

Clearing Faults on pg. 1

DRV.FAULTS on pg. 1, DRV.EN on pg. 1, DRV.DIS on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™