You are here: Tools > AKD into KAS > Workbench Reference > DRV.SETUPREQBITS

DRV.SETUPREQBITS

General Information

Type

R/O Parameter

Description

Reads the bitwise set status of parameters that must be set before the drive can be enabled.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Description

This parameter returns the bitwise set status of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.

The following table lists the parameters which require setup for each motor type.

Parameter Bit Default Value Linear Permanent Magnet Induction Motor V/f Open Loop Induction Motor Closed Loop Interior Permanent Magnet Brush Motor
IL"Instruction list" This is a low-level language and resembles assembly.KP 0 50 [V/A] √ - √ √ √
MOTOR.IPEAK 1 2 Arms √ √ √ √ √
MOTOR.ICONT 2 1 Arms √ √ √ √ √
MOTOR.POLES 4 6 √ √ √ √ -
MOTOR.LQLL 7 17mH - - - √ -
MOTOR.LDLL 8 17mH - - - √ -
MOTOR.KE 9 0 - - - √ -
MOTOR.IMTR 10 100ms - - √ - -
MOTOR.IMID 11 0 - - √ - -
MOTOR.VOLTRATED 12 230 Vrmsrms stands for root mean square (also known as the quadratic mean) - √ - - -
MOTOR.VRATED 13 0 - - - √ -
MOTOR.LISAT 14 25 x DRIVE.IPEAK - - - √ -
MOTOR.VRIDK1 15 0 - - - √ -
MOTOR.VRIDK2 16 0 - - - √ -
MOTOR.IDMAX 17 0.5 x MOTOR.IPEAK - - - √ -
IL.KDPRATIO 18 1 - - - √ -
MOTOR.PITCH 19 32 √ - - - -
MOTOR.VOLTMAX 20 480 Vrms - - - √ √

Related Topics

DRV.SETUPREQLIST on pg. 1, MOTOR.AUTOSET on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™