You are here: Tools > AKD into KAS > Workbench Reference > DRV.SETUPREQLIST

DRV.SETUPREQLIST

General Information

Type

R/O Parameters

Description

Reads the list of parameters that must be set before the drive can be enabled.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Description

This parameter returns the list of parameters that must be set before the drive can be enabled and also whether or not each one of those parameters is set. This list of parameters will vary depending on the value MOTOR.TYPE. The drive can only be enabled when all commands have a value of 0.

Example

-->DRV.SETUPREQLIST

IL"Instruction list" This is a low-level language and resembles assembly.KP 0

MOTOR.ICONT 0

MOTOR.IPEAK 0

MOTOR.POLES 0

-->

Related Topics

DRV.SETUPREQBITS on pg. 1, MOTOR.AUTOSET on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™