You are here: Tools > AKD into KAS > Workbench Reference > IL.DCMD

IL.DCMD

General Information

Type

R/O Parameter

Description

Reads the value of the d-component current controller inside the FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable".

Units

Arms

Range

± DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK)

Default Value

N/A

Data Type

Float

See Also

DRV.IPEAK on pg. 1

Start Version

M_01-00-00-000

Description

This command displays the d-component current command value of the current loop. This parameter is commonly used with IPM motors (MOTOR.TYPE = 6), where the d-component current is controlled for closed loop current regulation.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™