You are here: Tools > AKD into KAS > Workbench Reference > IL.FF

IL.FF

General Information

Type

R/O Parameter

Description

Reads the current loop overall feedforward value

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

See Also

IL.KBUSFF on pg. 1, IL.KVFF on pg. 1, IL.OFFSET on pg. 1, IL.FRICTION on pg. 1, IL.KACCFF on pg. 1

Start Version

M_01-00-00-000

Description

IL.FF reads the present current loop overall feed-forwardThis describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment value. It is the sum of the following feed-forward paths:

IL.FF is calculated using the following variables' values at the time it is called:

IL.FF = IL.KACCFF * Accelration Command + VL.KVFF * Velocity Command + IL.FRICTION (if motion is currently commanded) + IL.OFFSET (always) + IL.KBUSFF on pg. 1 * IL.BUSFF (if fieldbus connected)

For EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs:

IL.BUSFF is the injected current feedforward, which corresponds to Object 60B2h: Torque Offset on pg. 1. The scaling for the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist offset is done with 1/1000 rated torque. In AKD, a value of 1000 means DRV.ICONT on pg. 1 will be commanded in IL.BUSFF (if IL.KBUSFF is set to 1).

IL.KBUSSFF is a gain setting for the feedforward value IL.BUSFF. It needs to be set to greater zero to let IL.BUSFF take effect. IL.KBUSFF can be access by SDO object 50E2h/0.

The IL.BUSFF gain can be commanded through EtherCAT in all DS402 operating modes.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™