You are here: Tools > AKD into KAS > Workbench Reference > IL.KACCFF

IL.KACCFF

General Information

Type

R/W Parameter

Description

Sets current loop acceleration feedforward gain value

Units

mArms/(rad/s²) 

Range

0 to 39113.288 mArms/(rad/s^2)

Default Value

0 mArms/(rad/s²) 

Data Type

Float

See Also

IL.FF on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3426h/0

M_01-00-00-000

Description

This value sets the gain for the acceleration feedforward (a scaled second derivative of the position command is added to the current command value) .

This parameter is valid only in the position mode (DRV.OPMODE = 2).

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™