You are here: Tools > AKD into KAS > Workbench Reference > IL.MIFOLD

IL.MIFOLD

General Information

Type

R/O Parameter

Description

Sets the motor foldback current limit.

Units

A

Range

0 to 2147483.647 A

Default Value

N/A

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

35A4h/0

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.MIFOLD sets the output of the motor foldback algorithm. It is an artificial current, which can be higher or lower than the motor peak currentThe effective value of the peak current. When IL.MIFOLD becomes lower than the existing current limit (IL.LIMITP on pg. 1) it becomes the active current limit.

IL.MIFOLD decreases when the actual current is higher than motor continuous current and increases (up to a certain level) when the actual current is lower than the motor continuous current.

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™