You are here: Tools > AKD into KAS > Workbench Reference > IL.LIMITP

IL.LIMITP

General Information

Type

NV Parameter

Description

Sets the positive user (application-specific) current limit.

Units

A

Range

0 A to drive peak currentThe effective value of the peak current (DRV.IPEAK)

Default Value

DriveControl device for regulating the speed, torque and position of a motor peak current (DRV.IPEAK)

Data Type

Float

See Also

IL.LIMITN on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

356Eh/0

M_01-00-00-000

Description

This parameter sets the positive user limit clamp value of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (IL.CMD on pg. 1). The current command is additionally limited by the motor peak current setting (MOTOR.IPEAK on pg. 1) and by the present value of the foldback I²t peak motor current protection.

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™