|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the negative user (application-specific) current limit. |
|
Units |
A |
|
Range |
Negative drive peak currentThe effective value of the peak current (DRV.IPEAK) to 0 A |
|
Default Value |
Negative drive peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
356Fh/0 |
M_01-00-00-000 |
Description
This parameter sets the negative user limit clamp value of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (IL.CMD on pg. 1). The current command is additionally limited by the motor peak current setting (MOTOR.IPEAK on pg. 1) and by the present value of the foldback I²t peak motor current protection.
This current limit is overwritten by MT.FIXEDSTOPCURRENT while a fixed stop motion task is running in a negative direction. Once the motion task is complete, the limit is restored to the previous IL.LIMITN value.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|