You are here: Tools > AKD into KAS > Workbench Reference > MOTOR.IPEAK

MOTOR.IPEAK

General Information

Type

NV Parameter

Description

Sets the motor peak currentThe effective value of the peak current.

Units

mA

Range

0.200 to 1,000 A

Default Value

2.000 A

Data Type

Float

See Also

IL.LIMITP on pg. 1, IL.LIMITN on pg. 1

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

358Fh/0

M_01-00-00-000

Description

This parameter configures the drive for the motor's peak, instantaneous-rated current. MOTOR.IPEAK is used to limit clamp the magnitude of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing q-component current command (IL.CMD on pg. 1).

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™