You are here: Tools > AKD into KAS > Workbench Reference > IL.VUFB

IL.VUFB

General Information

Type

R/O Parameter

Description

Reads the measured voltage on the u-winding of the motor.

Units

V

Range

–1200*VBusScale to +1200*VBusScale

Default Value

N/A

Data Type

Integer

See Also

IL.VVFB on pg. 1

Start Version

M_01-00-00-000

Description

Reads the measured voltage on the u-winding of the motor.

Related Topics

Current Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™