|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
V |
|
Range |
–1200*VBusScale to +1200*VBusScale |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Description
The range for this parameter depends on whether the drive model is an MV/240 VAC or an HV/480 VAC.
The VBusScale parameter sets the drive model:
MV/240 VAC: VBusScale = 1
HV/480 VAC: VBusScale = 2
VBusScale is used for multiple parameter ranges that are model dependent, such as IL.KP.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|