You are here: Tools > AKD into KAS > Workbench Reference > IP.ADDRESS

IP.ADDRESS

General Information

Type

NV Parameter

Description

Gets/Sets the IP address of the drive.

Units

N/A

Range

0.0.0.0 to 255.255.255.255

Default Value

0.0.0.0

Data Type

IP Address

Start Version

M_01-04-05-000

AKD-C and AKD-N

Type

R/O Paramter

Description

This Parameter sets the IP address of the drive. If this parameter has not been set by the user, it will return 0.0.0.0.

By default, DHCP is active, and the drive will acquire an IP Address on its own. When the drive is in DHCP mode, IP.ADDRESS will return 0.0.0.0.

Notes:

If manually setting the IP.ADDRESS, the IP.SUBNET on pg. 1 and IP.GATEWAY on pg. 1must be set up. After the IP.RESET on pg. 1 command is issued, the new IP settings will be active only if IP.MODE on pg. 1 has been set to 1.

 

Recovering communications with a drive on an un-reachable IP address

Sometimes a drive may be configured for an IP Address, and the drive needs to be taken off-line, and bench tested, or otherwise used outside of its saved IP Settings. If IP.MODE has been set to 1 (using software defined static IP) the drive will boot up on an IP Address that may be unreachable with the host computer’s settings.

If the IP address prevents communication the IP settings can be reset to default by the following procedure:

  1. Set both rotary switches to 0
  2. Hold down button B1 (top-side of drive) for 5 seconds.

The display will flash 0.0.0.0 and then attempt to discover an address by DHCP. Without removing logic power from the drive, use Workbench to connect to the drive, reconfigure the IP address settings as desired, and store the values to non-volatile memory.

Related Topics

IP.GATEWAY on pg. 1 | IP.RESET on pg. 1 | IP.SUBNET on pg. 1 | IP.MODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™