|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0.0.0.0 to 255.255.255.255 |
|
Default Value |
0.0.0.0 |
|
Data Type |
IP Address |
|
Start Version |
M_01-04-05-000 |
|
AKD-C and AKD-N |
|
|---|---|
|
Type |
R/O Paramter |
Description
This parameter sets the IP subnet mask of the drive. This parameter determines what IP addresses the drive will be allowed to communicate with.
By default, DHCP is active, and the drive will acquire an IP address on its own. When the drive is in DHCP mode, IP.SUBNET will return 0.0.0.0.
The default value of the EtherNet/IP model is 255.255.254.000.
Notes:
- When the drive is in DHCP, the actual IP subnet mask will not be returned using this command. The value the user has stored will be returned.
- IP.SUBNET will only be used by the drive when IP.MODE = 1
If manually setting the IP.ADDRESS on pg. 1, the IP.SUBNET and IP.GATEWAY on pg. 1must be set up. After the IP.RESET on pg. 1 command is issued, the new IP settings will be active only if IP.MODE on pg. 1 has been set to 1.
Recovering communications with a drive on an un-reachable IP address
Sometimes a drive may be configured for an IP Address, and the drive needs to be taken off-line, and bench tested, or otherwise used outside of its saved IP Settings. If IP.MODE has been set to 1 (using software defined static IP) the drive will boot up on an IP Address that may be unreachable with the host computer’s settings.
If the IP address prevents communication the IP settings can be reset to default by the following procedure:
- Set both rotary switches to 0
- Hold down button B1 (top-side of drive) for 5 seconds.
The display will flash 0.0.0.0 and then attempt to discover an address by DHCP. Without removing logic power from the drive, use Workbench to connect to the drive, reconfigure the IP address settings as desired, and store the values to non-volatile memory.
Related Topics
IP.ADDRESS on pg. 1 | IP.GATEWAY on pg. 1 | IP.RESET on pg. 1 | IP.MODE on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|