You are here: Tools > AKD into KAS > Workbench Reference > MOTOR.IDMAX

MOTOR.IDMAX

General Information

Type

NV Parameter

Description

Maximum direct axis current.

Units

Arms

Range

0.2 to 1000

Default Value

0.5 * MOTOR.IPEAK

Data Type

Float

Start Version

M_01-11-00-000

Description

This parameter is supported for IPM motors (MOTOR.TYPE = 6). MOTOR.IDMAX is the maximum motor winding current in the direct (non-torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing) axis.

Related Topics

Motor | MOTOR.IPEAK on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™