|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
mH |
|
Range |
1 to 2^31 |
|
Default Value |
17.000 |
|
Data Type |
Float |
|
Start Version |
M_01-11-00-000 |
Description
This parameter is the motor line to line direct axis inductance. It is supported for the IPM motor type (MOTOR.TYPE = 6).
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.
Related Topics
Motor | MOTOR.LQLL on pg. 1 | IL.KPDRATIO on pg. 1
|
Copyright © 2015 Kollmorgen™ |
|