You are here: Tools > AKD into KAS > Workbench Reference > REC.RETRIEVEDATA

REC.RETRIEVEDATA

General Information

Type

R/W Parameter

Description

Retrieves the recorded data without the header.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.RETRIEVE, REC.RETRIEVEHDR, REC.RETRIEVESIZE

Start Version

M_01-00-00-000

Description

REC.RETRIEVEDATA retrieves a section of recorded data according to REC.RETRIEVESIZE from the received index; if no index is received, the drive retrieves the data from next section. An index is supplied to enable multiple retrieves and to give better control on the buffer in case of overflow.  If no index or a negative value is present, then the index is ignored.

WorkBench uses this parameter to retrieve the data continuously for real time recoding.

The size of the data returned by this command depends on the number set by REC.RETRIEVESIZE.

Use REC.RETRIEVE for complete recording information view.

Notes:

Example

The following example retrieves data from index 100 in the size of 10 (hence places 100 to 109 in the buffer)

REC.NUMPOINTS 1000

REC.RETRIVESIZE 10

REC.TRIG

REC.RETRIEVEDATA 100

Related Topics

Scope on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™