You are here: Tools > AKD into KAS > Workbench Reference > REC.RETRIEVEFRMT

REC.RETRIEVEFRMT

General Information

Type

R/W Parameter

Description

Sets the format for recorded data output.

Units

N/A

Range

0 to 1; 0 = Standard format, 1 = Internal format (high speed)

Default Value

1

Data Type

Integer

See Also

REC.RETRIEVE on pg. 1, REC.RETRIEVEDATA on pg. 1

Start Version

M_01-00-00-000

Description

Recorded data is transferred to the communication channel in one of two formats: standard or internal high speed. The standard (slower) format cannot be used for continuous recording, but is more easily read. The high speed format allows continuous data recording (needed for autotuning). WorkBench supports both formats.

Example

The following recorder data is in standard format:

10,1

IL"Instruction list" This is a low-level language and resembles assembly.FB,VL.CMD,VL.FB

-0.086,0.000,2.661

0.000,0.000,3.605

0.029,0.000,-0.486

 

The following recorder data is in internal format:

10,1

IL.FB,VL.CMD,VL.FB

F3-0x56,F30x0,F30xA65

F30x0,F30x0,F30xE15

F30x1D,F30x0,F3-0x1E6

Related Topics

Scope on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™