|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
recorder samples |
|
Range |
0 to 65,535 recorder samples |
|
Default Value |
1,000 recorder samples |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Description
This parameter sets the number of samples that REC.RETRIEVEDATA on pg. 1 returns.
WorkBench also uses this parameter to set the number of samples returned when retrieving the data continuously for RT recoding.
Use REC.RETRIEVE on pg. 1 for the complete recording information view.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|