|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-04-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5261h/0 |
M_01-04-01-000 |
Description
This parameter is used to change voltage thresholds to allow -07 drive types to work at an -06 drive type's voltage thresholds. For information on voltage ratings and drive types see AKD Models on pg. 1.
When the VBUS.HALFVOLT value is changed, the revised thresholds take effect immediately.
VBUS.HALFVOLT only affects -07 drives.
| Value | Description |
|---|---|
| 0 | The original voltage thresholds are used for the functions mentioned below. |
| 1 | -07 drives use voltage thresholds of -06 drives. |
This parameter has an impact on the following voltage-thresholds:
The DC-bus under voltage fault threshold (see VBUS.UVFTHRESH on pg. 1) is a user selectable command. It means that the user is responsible for setting the under voltage threshold to a proper value in case that the AKD is supplied with a lower DC-bus voltage than the rated voltage.
|
Copyright © 2015 Kollmorgen™ |
|