You are here: Tools > AKD into KAS > Workbench Reference > VL.KO

VL.KO

General Information

Type

R/W Parameter

Description

Scales the observer velocity signal; active in opmodes 1 (velocity) and 2 (position) only.

Units

Internal

Range

0 to 65,535

Default Value

0

Data Type

Float

See Also

VL.MODEL on pg. 1

Start Version

M_01-00-01-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

51B3h/0

M_01-00-01-000

Description

VL.KO is used to scale the observer model to match the load. When VL.KO is tuned properly, Reads the observer velocity signal; active in opmodes 1 (velocity) and 2 (position) only. on pg. 1 will match VL.FB on pg. 1, except when there is an unspecified offset between the two.

Related Topics

Velocity Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™