|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
Reads the observer velocity signal; active in opmodes 1 (velocity) and 2 (position) only. |
|
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR, UNIT.ACCLINEAR Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, μm/s, (custom units)/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-01-000 |
Description
VL.MODEL is the observer velocity output. When VL.KO on pg. 1 is tuned properly, VL.MODEL will match VL.FB on pg. 1, except when there is an unspecified offset between the two.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|