You are here: Technical References > Programming Languages > PLC Standard Libraries > CASE OF ELSE END_CASE

CASE OF ELSE END_CASE

Statement - switch between enumerated statements.

Syntax

CASE <DINT expression> OF
<value> :
    <statements>
<value> , <value> :
    <statements>;
<value> .. <value> :
    <statements>;
ELSE
    <statements>
END_CASE;

Remarks

All enumerated values correspond to the evaluation of the DINT expression and are possible cases in the execution of the statements. The statements specified after the ELSE keyword are executed if the expression takes a value which is not enumerated in the switch. For each case, you must specify either a value, or a list of possible values separated by comas (",") or a range of values specified by a "min .. max" interval. You must enter space characters before and after the ".." separator.

ST Language

(* this example check first prime numbers *)
CASE iNumber OF
0 :
   Alarm := TRUE;
   AlarmText := '0 gives no result';
1 .. 3, 5 :
   bPrime := TRUE;
4, 6 :
   bPrime := FALSE;
ELSE
   Alarm := TRUE;
   AlarmText := 'I don't know after 6 !';
END_CASE;

FBD Language

Not available

FFLD Language

Not available

IL Language

Not available

See also

IF   WHILE   REPEAT   FOR   EXIT

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™