You are here: Technical References > Programming Languages > PLC Standard Libraries > EXIT

EXIT

Statement - Exit from a loop statement

Remarks

The EXIT statement indicates that the current loop (WHILE, REPEAT or FOR) must be finished. The execution continues after the END_WHILE, END_REPEAT or END_FOR keyword or the loop where the EXIT is. EXIT quits only one loop and cannot be used to exit at the same time several levels of nested loops.

ST Language

(* this program searches for the first non null item of an array *)
iFound = -1; (* means: not found *)
FOR iPos := 0 TO (iArrayDim - 1) DO
   IF iPos <> 0 THEN
      iFound := iPos;
      EXIT;
   END_IF;
END_FOR;

FBD Language

Not available

FFLD Language

Not available

IL Language

Not available

See also

IF   WHILE   REPEAT   FOR   CASE

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™