You are here: KAS IDE Reference > Create Programs > FBD Editor > Select FBD Variables and Instances

Select FBD variables and instances

Press this button or press ESCAPE before any selection.

To select the name of the declared variable to be attached to a graphic symbol, you must be in "Selection" mode. Simply double-click on the tag-name gray area. The following types of object must be linked to valid symbols:

Block: If it is a function block, you must specify the name of a valid declared instance of the corresponding type. 

Variable: Must be attached to a declared variable. Alternatively, a variable box may contain the text of a valid constant expression. 

Label: Must have a name. The name must be unique within the diagram. 

Jump: Must have the same name as its destination label. 

Contact: Must be attached to a declared Boolean variable. 

Coil: Must be attached to a declared Boolean variable.

Symbols of variables and instances are selected using a variable list, that can be used as the variable editor. Simply enter a symbol or constant expression in the edit box and press OK. You can also select a name in the list of declared objects, or declare a new variable by pressing the "Create" button.

For more details, Select Variables and Instances

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™