You are here: KAS IDE Reference > Create Programs > FBD Editor

Function Block Diagram (FBD) Editor

The FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks Editor is a powerful graphical tool that enables you to enter and manages Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. Diagrams according to the IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard. The editor supports advanced graphic features such as drag-and-drop, object resizing and connection line routing features, so that you can rapidly and freely arrange the elements of your diagram. It also enables you to insert in a FBD diagram graphic elements of the FFLD (Ladder Diagram) language such as contacts and coils.

FBD diagram components Related sections
Function blocks
Variable tags
Comment texts
Corners
Network breaks
Labels
Jumps
Use of ST instructions
Using the FBD toolbar
Selecting function blocks
Drawing connection lines
Selecting and entering variables and FB instances
Viewing the diagram
Moving or copying parts of the diagram
Inserting an object on a line
Resizing objects
Bookmarks
FFLD components:  
Contacts
Coils
"OR" vertical rail
Power rails
 

Boolean connections can be negative at the entry of a block.

Execution order can be displayed.

Concept Link IconSee Also

 

The FBD Toolbar

Draw FBD Connection Lines

Select FBD Variables and Instances

View FBD Diagrams

Move or Copy FBD Objects

Insert FBD Objects on a Line

Resize FBD Objects


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™