You are here: KAS IDE Reference > Create Programs > FBD Editor > View FBD Diagrams

View FBD diagrams

The diagram is entered in a logical grid. All objects are snapped to the grid. The (x,y) coordinates of the mouse cursor are displayed in the status bar. This helps you to locate errors detected by the compiler, or to align objects in the diagram.

At any moment you can zoom in or out of the edited diagram by means of a Ctrl + mouse-wheel operation. You can also press the [+] and [-] keys of the numerical keypad to zoom the diagram in or out.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™