You are here: Tools > Human Machine Interface Editor > Using the Internal Editor > Graphic Objects Properties

Graphic Objects Properties

This page details all possible properties for graphic objects. Refer to the list of available objects for further information on which property is used for which object.

   

Identifier

You can freely attach a text identifier to each graphic object inserted in a document. Identifiers are useful for arranging overlapped objects as they appear in the "Z-order" list.

Variable symbol

It is the full name of the application variable connected to the graphic object. In case of a local variable, its symbol must be prefixed with the parent program name, separated with "/". Example: "MyProg/MyVar".

Spying delay

It is the minimum period for actuating the value of the connected variable, expressed as a number of milliseconds. If the delay is not specified or equal to 0, refresh is done as fast as possible.

Border size

This property indicates the width of the border drawn around the object, expressed as a number of pixels. If this property is 0, then no border is drawn.

Border color

This property indicates the color of the border drawn around the object.

Border style

This property indicates the possible 3D effect used for drawing the border around the object. Possible values are:

FLAT = no 3D effect
3DUP = depressed 3D effect
3DDOWN = pressed 3D effect
3D = default 3D effect

Text color

This property indicates the color used for inserting texts in the graphic object.

Text mode

This property indicates the font effect used for drawing texts in the graphic object. Possible values are:

HIDE = text is not displayed
NORMAL = normal font
BOLD = bold text
ITALIC = italic text
UNDERLINE = underlined text

Font name

This property indicates the name of the character font used for drawing texts in the graphic object.

Font size

This property indicates the size of the character font used for drawing texts in the graphic object. The size is expressed as a percentage of the actual height of the object. Maximum possible value is 100. This ensures that the ratio is kept when the object is resized.

Background color

This property indicates the color used for filling the background of the object. In case of a bitmap, it specifies the color that must not be drawn if the TRANS (transparent) background mode is specified.

Background mode

This property indicates whether the background of the object must be filled or not. If this property is OPAQUE, then the background is filled with the specified background color. If this property is TRANS (transparent) then the background is not filled. Transparent drawing mode can be useful in the case of overlapping objects.


  • Specifying the TRANS (transparent) mode for large bitmaps is time-consuming and will affect the real-time performances of graphic updates.

Data format

If defined, this property indicates that the value of the connected variable must be displayed on the graphic object. You must specify for this property a format string that indicates how the data will be formatted.


  • The "text" property is ignored when a data format is specified.

Format string has the same format as the famous "printf" function of "C" language. It can include static characters together with one of the following possible pragmas that specify the value:

%s = default formatting according to IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies syntax
%d = integer (decimal)
%X = hexadecimal
%g = floating point
%.nf = decimal real (n is the number of displayed decimal digits)

Below are some examples:

Format

Value

Displayed string

%d

12.3

12

Var = %g meters

1.2

Var = 1.2 meters

%.2f

1.12345

1.12

Text

If defined, this property indicates the text to be displayed on the graphic object.


  • This property is ignored when a data format is specified.

Bitmap display mode

For bitmap-based objects, this property indicates whether the attached bitmap must keep its original aspect or be stretched to the actual size of the object. Possible values are:

ORIGINAL = keep the original aspect of the bitmap (cut if too large)
STRETCH = stretch or shrink the bitmap for fitting the actual size of the graphic object


  • Large bitmaps with "STRETCH" display mode are time-consuming during animation and can lead to poor performance.

Minimum value

For analog animated objects (meters, bar graphs or trends) this property indicates the minimum possible value that can be displayed. For static scales, it indicates the value of the lowest mark.

Maximum value

For analog animated objects (meters, bar graphs or trends) this property indicates the maximum possible value that can be displayed. For static scales, it indicates the value of the highest mark.

Data color

This property indicates the color used to represent the value of a connected variable within the object (for example the filled part of a bar graph).

Nb divisions (main)

For objects including a graphic scale, this property indicates the number of main division marks to be drawn in the scale.

Nb divisions (small)

For objects including a graphic scale, this property indicates the number of small division marks to be drawn in the scale, between each main division mark.

Scale color

For objects including a graphic scale, this property indicates the color used for drawing the axis, the division marks and corresponding values of the scale.

Bitmap pathname

For bitmaps, this property specifies the pathname of the bitmap to be displayed. BMP, GIF and JPG formats are supported. If no directory is specified, the specified file name is searched:

Bitmap for "TRUE" state

For two-state objects having the "CUSTOM" aspect, this property specifies the pathname of the bitmap to be displayed when the value of the attached variable is TRUE (or not zero for analogs). BMP, GIF and JPG formats are supported. If no directory is specified, the specified file name is searched:

  • in the project folder
  • in the "\BITMAP" folder of the KAS IDE

Bitmap for "FALSE" state

For two-state objects having the "CUSTOM" aspect, this property specifies the pathname of the bitmap to be displayed when the value of the attached variable is FALSE (or zero for analogs). BMP, GIF and JPG formats are supported. If no directory is specified, the specified file name is searched:

  • in the project folder
  • in the "\BITMAP" folder of the KAS IDE

Color when not connected

For shapes, this property indicates the color used for filling shapes when no variable is attached to the graphic object.

TRUE color

For shapes, this property indicates the color used for filling shapes when the attached variable has the TRUE state, or non zero for analogs.

FALSE color

For shapes, this property indicates the color used for filling shapes when the attached variable has the FALSE state, or zero for analogs.

Direction (basic shapes)

For oriented shapes such as triangles, half ellipses or cylinders, this property indicates the direction of the drawing; to the left, to the right, to the top or to the bottom.

Direction (scale)

For scales, this property indicates the direction of the axis. If LEFT, the minimum value is on the left side. If RIGHT, the minimum value is on the right side.

Placement (scale)

For scales, this property indicates the location of the scale within the object rectangle: on the left, on the right, on the top or at the bottom.

Action (text)

Indicates the possible mouse actions for text boxes. The following values are possible:

STATIC = no mouse action
EDIT = double-click opens an edit box for entering the variable value

Action (switch)

Indicates the possible mouse action for switches. The following values are possible:

STATIC = no mouse action
PUSHBUTTON = the variable is forced to TRUE when pressed and to FALSE when released
SWITCH = the status of the variable is inverted when the button is pressed
ONESHOTBUTTON = same as switch, but the display continues to appear released

Direction (bar graph)

For bar graphs, this property indicates the growing direction: to the left, to the right, to the top or to the bottom.

Nb of points (trends)

For trend charts, this property indicates the maximum number of stored points. If the width of the object (in pixels) is less than this number, then oldest points are not visible.

Direction (slider)

For slider, this property indicates whether the slider is horizontal (RIGHT) or vertical (TOP).

Link

This property indicates the name of the target .GRA animated document for shortcuts. If no directory is specified in the link, then the file is searched in the project folder.

Aspect (shapes)

This property indicates the type of basic shape to be drawn. Possible aspects are:

CYLINDER = a 3D like cylinder
ELLIPSE = an ellipse
HALFELLIPSE = one half of an ellipse
GATE = a simple vector drawing for a valve
RECTANGLE = a rectangle
ROUNDRECT = a rectangle with rounded corners
TRIANGLE = a triangle

Aspect (switches)

This property indicates the type of switch to be drawn. Possible aspects are:

DEFAULT = a standard Windows-like push button
CUSTOM = a button with TRUE and FALSE drawings defined with bitmaps

Aspect (trend charts)

This property indicates the type of drawing for a trend chart. Possible aspects are:

POINT = only relevant dots are drawn
LINE = lines are drawn from point to point
HISTO = histogram style

Aspect (digits)

This property indicates the type of drawing for a digital meter. Possible aspects are:

DEFAULT = plain drawing
BEZEL = all segments have a 3D effect

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™