Enhanced Write Filter Operational Procedures using the command line

Protect the PAC Image with EWF

The EWF should be activated on the PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system after the system is running and the PAC configuration is complete. If you want to change the CF image (such as a new KAS version or downloading a new application), then turn off the EWF filter, make the change, and then reactivate EWF.

  1. Open a command prompt by pressing Start > Run and type: cmd
  2. From the command prompt, type: ewfmgr C: -enable
  3. Reboot the PAC to activate the EWF

To ensure that the command has been entered correctly, execute the DOS command shell ewfmgr c: prior to rebooting the PAC. Check the field Boot Command, which should be set to "ENABLE", as seen in the image below.

Perform Changes on a Protected Volume

The EWF has to be disabled to perform changes on a PAC. After the changes are made the EWF is re-enabled.

  1. Open a command prompt by pressing Start > Run and type: cmd
  2. From the command prompt, type: ewfmgr C: -commitanddisable
  3. Reboot the PAC to commit the changes and disable EWF
  4. Make the desired changes (program installation, files record, etc.)
  5. From the command prompt, type: ewfmgr C: -enable
  6. Reboot the PAC to activate the EWF

Perform Small Changes on a Protected Volume

To commit changes without disabling and re-enabling EWF, a single commit can be commanded:

  1. From the command prompt, type: ewfmgr C: -commit
  2. Reboot the PAC to commit the changes (EWF remains active).

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™