ECATCommErrorsThis function block returns a list of bad EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs connections. If EtherCAT network communication is shutdown, the failed connections are based on information that was taken at the time the network was shutdown.
Figure 11-188: ECATCommErrors function block
| Define | Port |
|---|---|
| #define EC_PORT_A | 0 (* Port A *) |
| #define EC_PORT_B | 1 (* Port B *) |
| #define EC_PORT_C | 2 (* Port C *) |
| #define EC_PORT_D | 3 (* Port D*) |
| Execute | Description | Read the communication errors on the rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge |
| Data type | BOOL | |
| Range | 0,1 | |
| Unit | n/a | |
| Default | — | |
|
Connection |
Description | Array of bad connections. The safe size for the list is [2 * (number of devices) - 1]. |
| Data type | ECATCommErr_ref (see ECATCommErr_ref Structure table above) | |
| Range | N= 0 to 2 times the number of EtherCAT devices. | |
| Unit | n/a | |
| Default | — |
| Done | Description | Indicates when the function is complete |
| Data type | BOOL | |
| Unit | n/a | |
|
Error |
Description | Indicates the function failed due to an error. |
| Data type | BOOL | |
| Unit | n/a | |
| ErrorID | Description | The function call error result, if Error is TRUE (see Possible Error Codes and Descriptions table below). Upon success, Error is set to zero.. |
| Data type | DINT | |
| Unit | n/a | |
| ConnectionCount | Description | The number of bad connections. Valid indices in the Connection array range from zero to ConnectionCount -1 (assuming that ConnectionCount != 0). |
| Data type | UINT | |
| Unit | n/a |
| Error Code | Description |
|---|---|
| ECERR_DEVICE_ERROR | The EtherCAT driver is in a bad state |
| ECERR_FEATURE_NOT_AVAILABLE | The feature is not available on the PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system |
| ECERR_INVALID_ARRAY_SIZE | The size of the Connections is too small |
(********************************************************)
Read EtherCAT communication errors.
(********************************************************)
commErrors( TRUE, Connection);
|
Copyright © 2015 Kollmorgen™ |
|