MC_StopRegist
|
En |
Description |
Enables execution |
|
Data type |
BOOL |
|
|
Range |
0, 1 |
|
|
Unit |
n/a |
|
|
Default |
— |
|
| Axis |
Description |
Axis registration to turn off |
|
Data type |
AXIS_REF | |
|
Range |
The range of .AXIS_NUM is [1,256] | |
|
Unit |
n/a | |
|
Default |
n/a | |
| TriggerInput |
Description |
Structure specifying the fast input to disarm. The structure elements are: InputID INT 0 = Capture Engine 0 1 = Capture Engine 1 Range is [0,1] For information on configuring the capture engines, refer to AKD Capture Engine Configuration. Direction INT TrigID INT
|
|
Data type |
TRIGGER_REF | |
|
Range |
||
|
Unit |
||
|
Default |
|
OK |
Description |
Indicates function executed successfully |
|
Data type |
BOOL |
To use Capture Engine 1 modify the input PDOs that are used and add the LatchThe control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT bus cycle. The status word is used to return the drive's latch status Position 1 parameter.
|
Copyright © 2015 Kollmorgen™ |
|