This button allows the creation of a new variable to be mapped to the selected item(s).
| Field | Description |
| Scope | Defines where the variable is created |
| Name | See Name a variable |
| Type | Defines the Type of the variable, and its Dimension if the variable is an array |
| Dimension | The dimension of the variable (read-only). The dimension is set automatically based on the necessary size and the selected variable type. |
| Init Value | See Initial Value of a Variable |
See also Create Variables
For integer variables with types stored on several bits, the Advanced button gives access to the Start bit definition. This allows you to link a set of channels to a specific range of bits within an integer variable.
For example, when you select three channels ranging from 1 to 3 and map them to a DINT variable (stored on 32 bits ranging from 0 to 31), the first channel can be linked to position ranging from 0 to 29.
The three channels are mapped to the last three bits ranging from 29 to 31.
|
Copyright © 2015 Kollmorgen™ |
|