Backup and Restore a PDMM or PCMM

The SD card is used for backing up and restoring the data from a PDMM or PCMM.

Backing up may be performed in either of two ways.

Restoring information to the controller may be performed in either of two ways. Both methods restore the controller (and PDMM drive) with whatever was saved to the SD card.

Backup & Restore What? To/From SD card via B2/B3 buttons To/From SD card via Web Server Import/Export to/from PC
Application Program  
Retain Variables  
Drive Firmware    
Controller Firmware      
EtherCAT Configuration  

About the data transfer

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™