Reset the Controller to Factory Settings

The PDMM or PCMM can be manually triggered to perform a factory reset. The reset is performed using either of two methods:

After two seconds have expired (or longer if pressed during power-up), the 7-segment display on the control will change to an animation pattern indicating that the factory reset has started.

The following changes occur during a factory reset:

Some important facts to remember:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™