|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0, 1, 3 |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
Description
DRV.ACTIVE reads the enable status of an axis as follows:
There is no state 2.
When the drive is in state 3, the drive display shows a blinking decimal point.
If an axis is not enabled (DRV.ACTIVE is 0), but DRV.EN is 1 and the hardware enable is high, read the value of DRV.DISSOURCES to query the reason that the drive is not enabled.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|