|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
Arms |
|
Range |
0 to 2,147,483.647 Arms |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3559h/0 |
M_01-00-00-000 |
Description
IL"Instruction list" This is a low-level language and resembles assembly.DIFOLD is the output of the drive foldback algorithm. It is an artificial current, which can be higher or lower than the drive peak currentThe effective value of the peak current (DRV.IPEAK). When IL.DIFOLD is lower than the existing current limit (such as IL.LIMITP ), it becomes the active current limit.
IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|