|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the positive user (application-specific) current limit. |
|
Units |
A |
|
Range |
0 A to drive peak currentThe effective value of the peak current (DRV.IPEAK) |
|
Default Value |
DriveControl device for regulating the speed, torque and position of a motor peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
356Eh/0 |
M_01-00-00-000 |
Description
This parameter sets the positive user limit clamp value of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (IL.CMD ). The current command is additionally limited by the motor peak current setting (MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.
This current limit is overwritten by MT.FIXEDSTOPCURRENT while a fixed stop motion task is running in a position direction. Once the motion task is complete, the limit is restored to the previous IL.LIMITP value.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|