|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
A |
|
Range |
0 to the minimum of user positive current limit (IL"Instruction list" This is a low-level language and resembles assembly.LIMITP) and motor peak currentThe effective value of the peak current (MOTOR.IPEAK).IL.LIMITP |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
IL.FF |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3422h/0 |
M_01-00-00-000 |
Description
Position command derivative sign is multiplied by this value to be injected to the current command.
IL.FRICTION is active in Position and Velocity modes (DRV.OPMODE = 1, 2), but not active in TorqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode (DRV.OPMODE = 0).
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|