|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3407h/2 354Bh/0 |
M_01-00-00-000 |
Description
This parameter sets the gain for the velocity feedforward (a scaled derivative of the position command is added to the velocity command value). The nominal feedforward value can be multiplied by this gain value.
This parameter is only used in the position mode (DRV.OPMODE = 2).
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|