VL.MODEL

General Information

Type

R/O Parameter

Description

Reads the observer velocity signal; active in opmodes 1 (velocity) and 2 (position) only.

Units

Depends on UNIT.VROTARY or UNIT.VLINEAR, UNIT.ACCLINEAR

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, μm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

See Also

VL.FB , VL.KO

Start Version

M_01-00-01-000

Description

VL.MODEL is the observer velocity output. When VL.KO is tuned properly, VL.MODEL will match VL.FB , except when there is an unspecified offset between the two.

Related Topics

Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™