VL.OBSMODE

General Information

Type

NV Parameter

Description

Sets the observer operating mode.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-03-00-004

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

51BBh/0

M_01-03-00-004

Description

This parameter sets the observer operating mode. When VL.OBSMODE = 0, the observer is not part of the control loop; that is, VL.FB is used as the velocity feedback signal to the velocity loop. When VL.OBSMODE = 1, the observer is part of the control loop; VL.MODEL is used as the velocity feedback signal.

Related Topics

Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™