VL.VFTHRESH

General Information

Type

R/O Parameter

Description

Reads the overall overspeed fault threshold.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-10-03-000

Description

This parameter reports the overall overspeed fault threshold. Whichever of the following thresholds has the smallest value is used as the overall overspeed fault threshold:

Related Topics

Velocity Loop | VL.THRESH | MOTOR.VMAX

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™