IN1 : ANY_NUM First input
IN2 : ANY_NUM Second
input
Q : ANY_NUM Result: IN1 / IN2
All inputs and the output must have the same type. In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the DIV instruction performs a division between the current result and the operand. The current result and the operand must have the same type.
Q := IN1 / IN2;
(* The division is executed only if EN is TRUE *)
(* ENO is equal to EN *)
Op1: FFLD IN1
DIV IN2
ST Q (* Q is equal to: IN1 / IN2 *)
Op2: FFLD IN1
DIV IN2
DIV IN3
ST Q (* Q is equal to: IN1 / IN2 / IN3 *)
See also
|
Copyright © 2015 Kollmorgen™ |
|