IN1 : ANY_NUM First input
IN2 : ANY_NUM Second input
Q : ANY_NUM Result: IN1 * IN2
All inputs and the output must have the same type. In FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks language, the block can have up to 16 inputs. In FFLD language, the input rung (EN) enables the operation, and the output rung keeps the same value as the input rung. In IL"Instruction list" This is a low-level language and resembles assembly language, the MUL instruction performs a multiplication between the current result and the operand. The current result and the operand must have the same type.
Q := IN1 * IN2;
(* the block can have up to 16 inputs *)
(* The multiplication is executed only if EN is TRUE *)
(* ENO is equal to EN *)
Op1: FFLD IN1
MUL IN2
ST Q (* Q is equal to: IN1 * IN2 *)
Op2: FFLD IN1
MUL IN2
MUL IN3
ST Q (* Q is equal to: IN1 * IN2 * IN3 *)
See also
|
Copyright © 2015 Kollmorgen™ |
|