Timers

Below are the standard functions for managing timers:

TON

On timer

TOF Off timer
TP PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated timer
BLINK Blinker
BLINKA Asymmetric blinker
PLS Pulse signal generator
TMU Up-counting stop watch
TMUsec Up-counting stop watch (seconds)
TMD Down-counting stop watch

These functions make use of the Time data type. See Data Types for more information.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™