For a description of the this pipe block and its parameters, see Pipe Blocks Description
| Name | Description | Return type |
| MLCNVConnect | Connects a converter Pipe Block to the specified axis | BOOL |
| MLCNVConnectEx | Connects an extra converter Pipe Block to the specified axis. This function connects the output of a pipe to an axis data other than the control position. | BOOL |
| MLCNVDisconnect | Disconnects a converter Pipe Block from its associated axis | BOOL |
| MLCNVInit | Initializes a converter Pipe Block in Position or Speed mode | BOOL |
|
Copyright © 2015 Kollmorgen™ |
|