ECATMasterStatusThis function block reads the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs master state and the lost frame counter, to determine if EtherCAT is running normally.
Figure 11-185: ECATMasterStatus function block
| EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. | Description | Request to read the ECAT master state and the lost frame count. Keeps continously reads the master state and the lost frame count as long as the Enable remains high. |
| Data type | BOOL | |
| Range | 0,1 | |
| Unit | n/a | |
| Default | — |
| Valid | Description | Indicates the values at the 'State' and LostFrameCount outputs are valid. |
| Data type | BOOL | |
| Unit | n/a | |
| Error | Description | Indicates error |
| Data type | BOOL | |
| Unit | n/a | |
| ErrorID | Description | Error code when when the function block failed due to error. |
| Data type | DINT | |
| Unit | n/a | |
| State | Description | Indicates the ECAT state of the Master. See State Defines for details |
| Data type | UINT | |
| Unit | n/a | |
| LostFrameCount | Description | Total cumulative number of cyclic frames sent with no-response since the ECAT started by calling the MLMoitonStart. Missing return frames will generate an A38 alarm. The Counter is reset to 0 when the MLMotionStart is called. |
| Data type | UDINT | |
| Unit | n/a |
State Defines
#define EC_STATE_NO_COMMUNICATION 0 (* 0x00 = No Communication to device *)
#define EC_STATE_INIT 1 (* 0x01 = Device in Init state *)
#define EC_STATE_PREOP 2 (* 0x02 = Device in Pre-operational state *)
#define EC_STATE_BOOTSTRAP 3 (* 0x03 = Device in Bootstrap state *)
#define EC_STATE_SAFEOP 4 (* 0x04 = Device in Safe-Operational state *)
#define EC_STATE_OP 8 (* 0x08 = Device in Operational state *)
ECATWCStatus, ECATDeviceStatus.
// ECATMasterStatus
Inst_ECATMasterStatus( True );
MasterSTate := Inst_ECATMasterStatus.State;
MasterLastFrameCount := Inst_ECATMasterStatus.LostFrameCount;
|
Copyright © 2015 Kollmorgen™ |
|